Linux Kernel 3.0 or above for IMX53 evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Kernel 3.0 or above for IMX53 evk board

Jump to solution
1,232 Views
kravik
Contributor IV


Hi,

I am using custom board based on IMX53 Evk, I want to use kernel 3.0 or above for the custom board. As per IMX53 users guide, Linux kernel 2.6.35 is available for Evk board, any other  3.x kernels also available for Evk board so that it can be ported to custom board.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
769 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ravi Kumar,

By now the newest BSP released in our website is L2.6.35_11_09_ER_SOURCE. About the kernel 3.0 or above you need to port it to your board yourself, no documents and BSP in our website.

And hope this link can help you, https://community.freescale.com/message/450096#comment-450096 .
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
770 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ravi Kumar,

By now the newest BSP released in our website is L2.6.35_11_09_ER_SOURCE. About the kernel 3.0 or above you need to port it to your board yourself, no documents and BSP in our website.

And hope this link can help you, https://community.freescale.com/message/450096#comment-450096 .
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply