Linux Drivers for SGTL5000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux Drivers for SGTL5000

Jump to solution
7,293 Views
anandmeharwade
Contributor II

Hi,

I am using I.MX6Q module in my design. Where could I get the Linux Drivers for SGTL5000 Audio codec

Please do share me the link for the same. For any more information feel free to reply me.

Regards

Anand Meharwade

Labels (2)
0 Kudos
Reply
1 Solution
5,995 Views
gary_bisson
Senior Contributor III
4 Replies
5,996 Views
gary_bisson
Senior Contributor III
5,994 Views
anandmeharwade
Contributor II

Dear Gary Bisson,

I have used your drivers for SGTL5000 and added into my software package. The device probing is successful and shows up the alsa device list.

When I run the 1kHz sine wave .wav file using aplay command, I am observing the signals on LINE OUT_L only and no signals at LINE OUT_R. Also the signal at LINE OUT_L is not as expected (>>>1Khz its varying frequency and doesn't look like sine wave)

Could you please let me if any other commands to be executed before running the aplay command.

For any clarification feel free to ask me. Thanks for the support

Thanks

Anand M

0 Kudos
Reply
5,994 Views
anandmeharwade
Contributor II

Hi Gary Bisson,

Thanks for sharing the links for the drivers. Appriciate your help and quick response.

Thanks

Anand M

5,994 Views
igorpadykov
NXP Employee
NXP Employee

also may be useful to look at programming guides on

Ultra-Low-Power Audio Codec|NXP 

Best regards
igor

0 Kudos
Reply