Licensing model for DSP Concepts Algorithm in i.MX 8M Development Kit AVS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Licensing model for DSP Concepts Algorithm in i.MX 8M Development Kit AVS

1,553 Views
contact4
Contributor I
1. Wanted to enquire regarding the licensing model for the DSP Concepts Audio Algorithms Licensing model with NXP and NXP’s future customers
2. Licensing model for Sensory WWE for "Alexa"
Also shall be using this kit to develop a smart home voice enabled device and thereby might require support for following 
1. Support for porting our current application from Debian 9 to supported OS (Like building few libraries/packages which might not be there in new OS)
2. Support for Hardware compatibility ( for example adding a MIPI Display)
Labels (1)
0 Kudos
Reply
1 Reply

1,406 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ashwani Agrawal,

The 32 bits version can be renewed every couple of months. There is no public test for the 64-bits version. In both cases you may contact DSP Concepts for more information on available licenses.

In the case of Sensory you would also need to contact them directly for licensing details.

As for support for Debian 9 it is not currently implemented so you may either port the application yourself or you may contact NXP Professional Services to quote the porting job.

Regarding Hardware compatibility with MIPI Display the i.MX8M does support MIPI display.

I hope this information helps!

Regards,

0 Kudos
Reply