Large Code Size of M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Large Code Size of M4

1,644 Views
zhiqunhu
Contributor III

As I have seen so far, all the notes and examples of Cortex M4 of iMX7D are using uBoot in A7 to load the code into TCM (I guess OCRAM could be used for that as well) and then run from there.

But if the code size of M4 is 512k+, can a separated DDR or SRAM be assigned to M4 so uBoot can load the code into it and run from there for M4? If not, if the code size is larger than OCRAM, how to handle the situation?  

Labels (1)
0 Kudos
Reply
2 Replies

1,514 Views
igorpadykov
NXP Employee
NXP Employee

Hi Zhiqun

one can look on imx-m4fwloader loading m4 code from Linux.

GitHub - NXPmicro/imx-m4fwloader: Tool for loading firmware to M4 core on i.MX6SX and 7D 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,514 Views
zhiqunhu
Contributor III

I have read APP note of An5127, so the same DDR can be used by both A7 and M4, not sure how does that work yet. 

0 Kudos
Reply