LVDS output problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS output problem

1,902 Views
thouswave
Contributor III

Hi

Now, My project uses two channel LVDS to output 1080P image, and use an FPGA to sample。

Now,my problem is that we can test waveform from CHx_DATA0,CHx_DATA1,CHx_DATA2, but can not get any wave form from CHx_DATA3?

The following is my LVDS config in bsp:

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

  {

  .disp_dev = "lvds-lcd",

  .interface_pix_fmt = IPU_PIX_FMT_RGB32,

  .mode_str = "LDB-XGA",

  .default_bpp = 32,

  .int_clk = false,

  .late_init = false,

  },

};

static struct fsl_mxc_ldb_platform_data ldb_data = {

  .ipu_id = 0,

  .disp_id = 1,

  .ext_ref = 1,

  .mode = LDB_SPL_DI1,

  .sec_ipu_id = 0,

  .sec_disp_id = 0,

};

Can anyone give me some idea?

0 Kudos
Reply
1 Reply

1,743 Views
igorpadykov
NXP Employee
NXP Employee

Hi 千

I would suggest to look at link below with example which supports 1080p lvds lcd

http://boundarydevices.com/jellybean-max/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply