LTIB kernel contribution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB kernel contribution

2,960件の閲覧回数
alexsmirnov
Contributor II

Dear Freescale,

I work with i.MX6 SoC and walking through the kernel I've found several issues. I'm familar with kernel development community due to have a huge experience contributing to mainline, but does Freescale provide some infrastructure to contribute LTIB BSP?

With best regards,

Alex

4 返答(返信)

2,526件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

It would be very nice to have you in meta-freescale project, alexsmirnov!

We can include your kernel patches or any other patch you have!

Please, register your self https://lists.yoctoproject.org/listinfo/meta-freescale

As Leo mentioned, a lot help is needed :smileywink:

0 件の賞賛
返信

2,526件の閲覧回数
LeonardoSandova
Specialist I

Hi Alex,

Do your want to contribute to freescale kernel repo? or BSP in general? For the BSP case, this year (I am not sure when), we are moving to Yocto, which as you know, this is an open-source project and you can (of course) contribute to it (check this link). A lot of help is needed!. I would recommend that your efforts go into this direction.

Leo

0 件の賞賛
返信

2,526件の閲覧回数
alexsmirnov
Contributor II

Dear Leonardo,

thank you for the reply. Unfortunately I'm not familar with Freescale development processes and which kernel trees do you use internaly. My situation is following: I work with i.MX6 SoC and have tried the latest LTIB from Freescale downloads. I've found several issues in the code and want to share my fixes. But I don't know any Freescale trees, mail-lists etc..

Alex

0 件の賞賛
返信

2,526件の閲覧回数
LeonardoSandova
Specialist I

FabioEstevam would be the best person to answer this question.

0 件の賞賛
返信