LTIB build error for i.mx53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB build error for i.mx53

1,389 次查看
akhiljhanwar
Contributor I

I am using LTIB to build rootfs for i.mx53 platform. I am using ubuntu 10.04 as host machine but when I run ./ltib I am getting the following error

Build path taken because: download only, no prebuilt rpm,

Testing network connectivity

No network download connection available

Can't get: rpm-4.0.4.tar.gz at ./ltib line 790.

could not glob rpm in: /tmp/rpm-akhil/RPMS/i686/rpm-fs-* at ./ltib line 2408.

traceback:

main::check_rpm_setup:2408

main::host_checks:1423

main:542

These packages failed to build

I think it is not detecting network proxy, how to change the proxy in .ltibrc file(I am not finding this file as mentioned in docs.)

标签 (2)
0 项奖励
回复
1 回复

1,151 次查看
SergioSolis
NXP Employee
NXP Employee

Hello,

You may want to try to edit the etc/enviroment file.

Yoy can set the proxy values in that file.

0 项奖励
回复