Hi,
I'm building a rootfs based upon ltib vL2.6.31_09.12.01 for the MX35 3stack EVK.
When I deploy the rootfs there's no gpu.o/gpu.ko available.
Also in the kernel config there's no option to enable -kernel- GPU support
(The userspace packages amd-gpu-bin-mx35 and libz160-bin are both enabled so there's no issue there)
In version 10.2010 of ltib, using L2.6.35, there is a MXC_AMD_GPU option available, however the IPU build for MX35 in this LTIB version is broken so I can't use that LTIB version either.
Did any of you manage to enable the amd-gpu kernel driver for MX35 with ltib ?
Thanks,
Christophe