LTIB Configuration error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LTIB Configuration error

2,644件の閲覧回数
ManojCR
Contributor I

Hi,

 

We are trying to enable the USB webcam for IMX51 EVK using the isntructions given in imX51 wiki.

As a first step we installed LTIB and then when we give ./ltib -c command it gives the error

 

"Error 1
make[2]: Leaving directory `/tmp/rpm-ubuntu/BUILD/rpm-4.0.4/tools'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/tmp/rpm-ubuntu/BUILD/rpm-4.0.4'
make: *** [all-recursive-am] Error 2
error: Bad exit status from /media/disk/L2.6.31_10.07.11_ER_source/y/ltib/tmp/rpm-tmp.54676 (%build)


RPM build errors:
    Bad exit status from /media/disk/L2.6.31_10.07.11_ER_source/y/ltib/tmp/rpm-tmp.54676 (%build)
Build time for rpm-fs: 1435 seconds

Failed building rpm-fs
could not glob rpm in: /tmp/rpm-ubuntu/RPMS/armv7l/rpm-fs-* at ./ltib line 2408.
traceback:
 main::check_rpm_setup:2408
  main::host_checks:1423
   main:542


Started: Tue Oct 26 06:36:08 2010
Ended:   Tue Oct 26 07:00:08 2010
Elapsed: 1440 seconds

These packages failed to build:
rpm-fs

Build Failed "

 

 

Please let me know the reason for this errors.

 

 

Aslo please help if there is any other way to enable the camera drivers.

 

Thanks,

Manoj

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,480件の閲覧回数
bonzo
NXP Employee
NXP Employee
Manoj, use the two shell script files located elsewhere in imxcommunity.org (http://imxcommunity.org/group/ubuntutipsandtricks/forum/topics/ltib-on-ubuntu-910). They work great. When you download them, be sure to change their attributes to executable, i.e. chmod +x ltib_installx this works great for Ubuntu 10 as well.
0 件の賞賛
返信

2,480件の閲覧回数
ManojCR
Contributor I
Hi Brad, Am using Linux ubuntu-desktop 2.6.28-474-gbd04b06 and ubuntu version is Ubuntu 9.04-the Jaunty Jackalope release. Am not using any SDK for buidling. Thanks, Manoj

Brad Stewart said:
What Linux are you using?
What SDK?
0 件の賞賛
返信

2,480件の閲覧回数
bonzo
NXP Employee
NXP Employee
What Linux are you using? What SDK?
0 件の賞賛
返信