LPDDR4 tuning on DDR tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR4 tuning on DDR tool

2,205件の閲覧回数
kevincheng
Contributor IV

Hi,

We use DDR tool 2.1 to tuning our new LPDDR4 memory on iMX8MQ. That pass the Calibration, and do the stress test, the result is fail. When we check "Disable DDR Memory Cache", and retest again, it pass. Then we direct use "Gen Code" and compiler with uboot, the result is my system sometime boot success and sometime boot fail on memory panic. Have any thing we can change on DDR tool or ds file?

1.png

Regards,

Kevin

ラベル(1)
0 件の賞賛
返信
1 返信

1,934件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Disable DDR Memory Cache option,  when selected,  means, that DDR memory

is mapped as none-cacheable/none-buffable memory when you run stress test.

When using the cache the memory is heavy loaded; such configuration corresponds  

OS working. Therefore it makes sense to check the memory more carefully, using

the  Hardware Developer’s Guide.

https://www.nxp.com/docs/en/user-guide/IMX8MDQLQHDG.pdf 

In particular, use  section 3.(i.MX 8MDQLQ layout/routing recommendations)

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------