Hello Guys,
i'm working with the adc_etc Hardware example. I tried it with the LPADC1 and both Conversions are working.
Then i switched to LPADC2 and did the neccessary XBAR changes usw. Now i only get one Result. The resulting conversion is the One that is choosen by the DEMO_ADC_USER_CHANNEL.
The other Conversion always stays at 0. If i change the DEMO_ADC_USER_CHANNEL to the second Input it works, but the first conversion stays zero.
Did i forgot something to configure? All i changed was the LPADC, the TriggerMask, Trigger Group and the XBAR output...
kind regards
Andy
Hi @Andy_h
Hope you are doing well.
Since there is no response on this thread, I am closing this ticket.
If you have any further questions, Please raise a new ticket.
Thanks & Regards
Sanket Parekh
Hi @Andy_h
I hope you are doing well.
Can you please share the below mentioned details?
-> Which processor you are using?
-> Configuration details of ADC
-> Connection diagram of ADC with processor.
Thanks & Regards
Sanket Parekh