LPADC2 Adc_Etc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPADC2 Adc_Etc

404 次查看
Andy_h
Contributor II

Hello Guys,

 

i'm working with the adc_etc Hardware example. I tried it with the LPADC1 and both Conversions are working.

Then i switched to LPADC2 and did the neccessary XBAR changes usw. Now i only get one Result. The resulting conversion is the One that is choosen by the DEMO_ADC_USER_CHANNEL. 

The other Conversion always stays at 0. If i change the DEMO_ADC_USER_CHANNEL to the second Input it works, but the first conversion stays zero.

Did i forgot something to configure? All i changed was the LPADC, the TriggerMask, Trigger Group and the XBAR output...

 

kind regards

Andy

0 项奖励
2 回复数

373 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Andy_h 

Hope you are doing well.

Since there is no response on this thread, I am closing this ticket.

If you have any further questions, Please raise a new ticket.

Thanks & Regards

Sanket Parekh

0 项奖励

378 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Andy_h 

I hope you are doing well.

Can you please share the below mentioned details?

-> Which processor you are using?

-> Configuration details of ADC

-> Connection diagram of ADC with processor.

Thanks & Regards

Sanket Parekh

0 项奖励