LPADC2 Adc_Etc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPADC2 Adc_Etc

1,622件の閲覧回数
Andy_h
Contributor II

Hello Guys,

 

i'm working with the adc_etc Hardware example. I tried it with the LPADC1 and both Conversions are working.

Then i switched to LPADC2 and did the neccessary XBAR changes usw. Now i only get one Result. The resulting conversion is the One that is choosen by the DEMO_ADC_USER_CHANNEL. 

The other Conversion always stays at 0. If i change the DEMO_ADC_USER_CHANNEL to the second Input it works, but the first conversion stays zero.

Did i forgot something to configure? All i changed was the LPADC, the TriggerMask, Trigger Group and the XBAR output...

 

kind regards

Andy

0 件の賞賛
返信
2 返答(返信)

1,591件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Andy_h 

Hope you are doing well.

Since there is no response on this thread, I am closing this ticket.

If you have any further questions, Please raise a new ticket.

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信

1,596件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Andy_h 

I hope you are doing well.

Can you please share the below mentioned details?

-> Which processor you are using?

-> Configuration details of ADC

-> Connection diagram of ADC with processor.

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信