LOCSC Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LOCSC Interface

2,993 Views
rubensjunior
Contributor IV

Dear collegues! Happy 2020!

Does anyone know of an interface called locsc for NXP processors?

Best regards.

Rubens Júnior.

3 Replies

2,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rubens

I never heard that such interface was used with i.mx processors, could you provide

some additional info or links about that interface.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,871 Views
rubensjunior
Contributor IV

Hi igorpadykov,

The LOCSC is a CMOS interface (No NXP).

I need to migrate a project that uses a LOCSC to CMOS Sensor Interface (CIS) using the iMXRT1051 processor. How I do?

Best Regards,

Rubens Júnior

0 Kudos
Reply

2,871 Views
igorpadykov
NXP Employee
NXP Employee