LDO configuration on DA9053

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LDO configuration on DA9053

ソリューションへジャンプ
1,305件の閲覧回数
IvoKamalis
Contributor I

Hi!

We are working on i.mx53 device similar to sabre. I want to ask about power supply. We chose DA9053. How and when the LDO output voltages are being configured. Do we need to program PMIC before or it is being configured from software running on i.mx53 SoC?I tried to find useful information on site but did not get the picture.

Thank you!


ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
989件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ivo,

The PMIC startup defaults are configured in the factory. When you purchase it, you have to specify these values so Dialog customize the ICs for you.

Best regards.

Jorge.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
990件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ivo,

The PMIC startup defaults are configured in the factory. When you purchase it, you have to specify these values so Dialog customize the ICs for you.

Best regards.

Jorge.

0 件の賞賛
返信
989件の閲覧回数
IvoKamalis
Contributor I

Thank you Jorge for your answer!

This sounds reasonable.

OK than one way is to order ic's with right voltages. I read in documentation that there is some way of programming voltage levels by programming OTP on this power chip. Does anyone have tried procedure like this and what equipment/software is needed?

0 件の賞賛
返信
989件の閲覧回数
kishan
Contributor II

Hi,

you don't need any equipment for that. You need to change appropriate register values to change voltage levels.

You can refer da9053 datasheet for such information.

Regards,

Kishan

0 件の賞賛
返信