LCD preview issue after HDMI Display start

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD preview issue after HDMI Display start

5,010件の閲覧回数
jignesh1
Contributor I

Hi all,

We are using imx6q processor with TM050RVHG01-00 LCD and using kernel version : 3.14.28 .

We have following issue.

1. After booting system, if we run LCD preview then it is correct as you find in attachment.

2. After booting system, first we run HDMI preview and then LCD preview then LCD preview gets corrupted. This corrupted also found in attachment.

3. After booting system, if we start both LCD and HDMI preview together then also we face same issue.

Following is the device tree of our product. we are using mxcfb1 for LCD and mxcfb2 for HDMI. Let us know if we are missing anything to configure IPU.

        mxcfb1: fb@0 {
                compatible = "fsl,mxc_sdc_fb";
                disp_dev = "lcd";
                interface_pix_fmt = "RGB24";
                mode_str ="TM050RVHG01-00";
                default_bpp = <24>;
                int_clk = <0>;
                late_init = <0>;
                status = "okay";
        };

        mxcfb2: fb@1 {
                compatible = "fsl,mxc_sdc_fb";
                disp_dev = "hdmi";
                interface_pix_fmt = "RGB24";
                mode_str ="1920x1080M@60";
                default_bpp = <32>;
                int_clk = <0>;
                late_init = <0>;
                status = "okay";
        };

We are using standard V4L2 base application to get preview on LCD and HDMI. So let us know if you need application source code.

Thanks,

Jignesh R Patel

タグ(1)
0 件の賞賛
返信
5 返答(返信)

4,905件の閲覧回数
jignesh1
Contributor I

Hi All,

Please help me for this. One more information I got that when I start HDMI output then it show following message.

imx-ipuv3 2400000.ipu: IPU DMFC DC HIGH RESOLUTION: 1(0~3), 5B(4,5), 5F(6,7)

So after this message I do see issue on LCD.

Thanks,

Jignesh R Patel

0 件の賞賛
返信

4,905件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jignesh

please try kernel boot parameter dmfc=3

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,905件の閲覧回数
jignesh1
Contributor I

Hi Igor,

Thanks for reply. I set bootargs as you mention but I got worst display output at HDMI and LCD.

Please find LCD and HDMI preview snapshot in attachment.LCD_with_dmfs3.jpg

hdmi_with_dmfc3.jpg

Let me know if any setting I am missing.

Thanks,

Jignesh Patel

0 件の賞賛
返信

4,905件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jignesh

please try to reproduce issue on nxp Sabre reference board.

Best regards
igor

0 件の賞賛
返信

4,905件の閲覧回数
jignesh1
Contributor I

Hi igor,

We do not have Sabre board. we have wand board but that does not support LCD. So please advice us if any alternative.

Default as I mention only LCD preview is working correct but issue start after I start HDMI preview. We have 800x480 resolution for LCD and 1920x1080 resolution for HDMI.

Thanks,

Jignesh Patel

0 件の賞賛
返信