LCD and hdmi dual display problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD and hdmi dual display problem

3,263件の閲覧回数
yyuan
Contributor III

hi

LCD and hdmi dual display problem。

i want to display on lcd and hdmi.

kernel is 4.1.15.

the LCD resolution is 1024x600,  the hdmi resolution is 1920x1080.lcd is fb0,hdmi is fb2.

lcd and hdmi is ok alone. but  together is not ok.

I want LCD and hdmi to show the same thing,such as qt 、video and real-time camera image.

what should i do?

please help me.

thank you.

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

3,083件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi  袁 野

what bsp used in the case, one can try nxp official L4.1.15 from

linux-imx - i.MX Linux kernel 

this configuration works fine as described in attached Linux Guide p.26 using

boot command line:

U-Boot > setenv displayinfo 'video=mxcfb1:dev=ldb video=mxcfb0:dev=hdmi,
1920x1080M@60,if=RGB24' for LVDS and HDMI dual displays

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,083件の閲覧回数
yyuan
Contributor III

hi igorpadykov

thank you

now i set displayinfo, it is right.but hdmi is not display.

images are displayed only on LCD.

i want to can display on LCD and hdmi together.

i want to know how to do it.

please help me 

thank you

0 件の賞賛
返信

3,083件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please try nxp official L4.1.15 from

linux-imx - i.MX Linux kernel 

Best regards
igor

0 件の賞賛
返信

3,083件の閲覧回数
yyuan
Contributor III

thank you

you mean let me download this kernel?

i have kernel 4.1.15.

i don`t why download the kernel?

please help me

thank you

0 件の賞賛
返信