LCD 480x272

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD 480x272

3,400件の閲覧回数
Nagraj
Contributor I
Im using Imx233 processor which has the lcd 3.5" 320x240 for 16 bit working, I modified the same driver code for 4.3" with 8 bit when trying to see the image(480x272 size) using imgtool the 480 lines are completly used but the out of 272 some 12 pixels rectangular shape is black screen as attached images(original and the 4.3" display image).I am using the framebuffer of 480x272 size? Thanks in advance.
タグ(2)
0 件の賞賛
返信
0 返答(返信)