LBEE5XV1YM WI-FI Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LBEE5XV1YM WI-FI Module

3,794件の閲覧回数
sanketparekh
Contributor II

Hi,

We are looking for the Wi-Fi module to be interfaced with iMX6DL processor. For the same, we have shortlisted the Murata LBEE5XV1YM module which is using the NXP 88W8997 chipset inside.

1. Is Linux kernel driver of LBEE5XV1YM module is provided by NXP/Module Vendor?
2. Is Linux driver available on 4.1.15 Linux kernel?
3. Please respond to the below queries related to our product requirements in context of LBEE5XV1YM module and Driver support
    a. To run the AP+STA simultaneously, is there any known limitation or a sequence of proper steps needs to be followed?
    b. Regarding the AP+STA mode, We wanted to understand the behavior of the module in the below use cases,
        Case 1:
        The module is configured and running as AP on channel number 1(2.412 GHz). When the module performs the scan as a STATION, which frequency AP list will be received in the scan request? (Only 2.4 GHz APs or both 2.4 and 5 GHz APs).
        Case 2:
        The module is configured and running as AP on channel number 1(2.412 GHz). What steps do we need to perform to connect the module as STATION with the external AP running on 5GHz?

 

Thanks & Regards.

Sanket Parekh

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,669件の閲覧回数
sanketparekh
Contributor II

Hi Igor,

Thank you for the reply.

I am looking for the test utility for FCC certification of WIFI module LBEE5XV1YM. Please share the FCC test utility for the same.

Thank you

Sanket

0 件の賞賛
返信

3,605件の閲覧回数
sanketparekh
Contributor II

Hi Igor,

Gentle reminder for the FCC test utility. We are planning to visit the FCC Lab on 13th of December.

Please share the FCC test utility ASAP.

Thank you.

 

0 件の賞賛
返信

3,783件の閲覧回数
sanketparekh
Contributor II

Hi Igor,

Thank you for quick response.

Can you please provide the details for queries mentioned below.

1. Please respond to the below queries related to our product requirements in context of LBEE5XV1YM module and Driver support
    a. To run the AP+STA simultaneously, is there any known limitation or a sequence of proper steps needs to be followed?
    b. Regarding the AP+STA mode, We wanted to understand the behavior of the module in the below use cases,
        Case 1:
        The module is configured and running as AP on channel number 1(2.412 GHz). When the module performs the scan as a STATION, which frequency AP list will be received in the scan request? (Only 2.4 GHz APs or both 2.4 and 5 GHz APs).
        Case 2:
        The module is configured and running as AP on channel number 1(2.412 GHz). What steps do we need to perform to connect the module as STATION with the external AP running on 5GHz?

Thanks & Regards.

Sanket Parekh

0 件の賞賛
返信

3,788件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sanket

 

88W8997 drivers are provided in latest nxp linux releases (but not L4.1.15) as described in

Table 50. On-board chips and external solutions for Bluetooth and Wi-Fi support   i.MX Linux Reference Manual​

For configuration one can look at 88W8997 docuemntation below, in particular UM11483

Getting Started with NXP-based Wireless Modules

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth/2-4-5-ghz-dual-band-2x2-wi-fi-5-802-11ac-...

 

Best regards
igor

0 件の賞賛
返信