LBEE5KL1PJ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LBEE5KL1PJ

7,825 Views
idom
Contributor II

I redesign the i.MX 8M Mini LPDDR4 EVK Board, and I want to use LBEE5KL1PJ.

I didn't find to much information about it.

  • datasheet
  • user guide
  • how can I purchase it.

the only info I found is this link

https://wireless.murata.com/datasheet?/RFM/data/lbee5zz1pj.pdf

I couldn't find info about QCA9377

Pls advice

Ido

0 Kudos
Reply
5 Replies

6,982 Views
romitchatterjee
Contributor V

Hello, actually, the 1PJ module is no longer supported. So it would be better if you use one of the newer modules with better support. For example, the Murata Type 1MW (https://wireless.murata.com/type-1mw.html ) would be a great option for you. 1MW also has SDIO based interface and provide 802.11ac+BT 5.0, just like 1PJ, so it will work with i.MX 8M Mini very well. Refer to the Murata Quick Start guide on details of how to bring it up: https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_linux.pdf .

6,982 Views
romitchatterjee
Contributor V

Hello Ido,

Murata 1PJ module resources (datasheet, purchase information) are available at: https://wireless.murata.com/type-1pj.html . Although the order number is different from what you mention, it does use the QCA9377 module.

Hopefully this will help.

Thanks.

6,982 Views
idom
Contributor II

whats the difference between the LBEE5ZZ1PJ and LBEE5KL1PJ?

I had the P\N from imx8 eval board.

why is datasheet preliminary?

On Thu, Sep 12, 2019 at 4:22 PM romitchatterjee <[email protected]>

0 Kudos
Reply

6,982 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ido,

This module is manufactured and supported by Murata, so I would recommend contacting them directly asking for the technical information available and purchase information.

My apologies for the inconvenience.
Regards,

0 Kudos
Reply

6,982 Views
idom
Contributor II

Thanks for your reply

0 Kudos
Reply