LAN95 (smsc95xx) causing data corruption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LAN95 (smsc95xx) causing data corruption

1,955 Views
ciaran_lequeux
Contributor I

Hi,

I have a custom board with imx6 dual lite, i'm on linux.

I have a problem with data corruption in ftp download.

For my tests, in bash, i download, check md5sum and loop...

With direct network connection, i download from ftp à big file (1GB), 100% OK of all time

Now with usb ethernet adapter (LAN95), (i dissabled turbo mode, otherwise it crash)

With a 1GB file FTP : KO 100% of time
With a 60Mb file  FTP : KO 1 / 10 of time
With 1GB file with SCP : KO 1 / 5 of time

Did you have any idea why isn't working properly ?

0 Kudos
Reply
2 Replies

1,886 Views
ciaran_lequeux
Contributor I

Hi,

 

Thanks you, but on his thread he says it's ok LAN to LAN, his command not work wih me and i'm LAN to LAN.

It's a ctusom board and i can't connect other adapters

 

I've already test with this parameters from uboot : [U-Boot] [PATCH] smsc95xx: Fetch whole burst with 1 URB, avoid framing errors (kernel.org)

Without success

 

0 Kudos
Reply

1,923 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Do the connections advise the same capabilities?

Could you try this setting?

I could also watch this instability here,

Have you worked with other adapters?

Regards

0 Kudos
Reply