L2 Cache as OCRAM (imx6ulz)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

L2 Cache as OCRAM (imx6ulz)

1,336件の閲覧回数
gingerologist
Contributor II

newbie to imx6 platform.

 

In the reference manual of imx6ulz, I noticed that L2 cache could be used as OCRAM. Does this mean if MMU is not used and the processor is intentionally used only with uboot, or some RTOSes (if any), rather than booting into a Linux system, there are totally 256KB sram available (128KB OCRAM + 128KB L2 cache)? If so, what is the memory address of "L2 cache as OCRAM"? I found only one region of OCRAM in Table 2-1. System memory map, in rm. Or I got it wrong. The 128KB OCRAM and the L2 Cache are the same device configured as different working mode?

タグ(1)
0 件の賞賛
返信
1 返信

1,272件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @gingerologist,

Please refer to this link for more information.

 

Best Regards,
Dhruvit.

0 件の賞賛
返信