Kit Kat 4.4 Build Issue With Libcamera2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kit Kat 4.4 Build Issue With Libcamera2

2,019件の閲覧回数
freewaymad
Contributor IV

Hi,

 

I am compiling a custom ROM based on Kit Kat 4.4.2. I am getting this error (excerpt from log; full log attached):

 

target SharedLib: camera.imx6 (out/target/product/sabresd_6dq/obj/SHARED_LIBRARIES/camera.imx6_intermediates/LINKED/camera.imx6.so)

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:118: error: undefined reference to 'ResetJpgfile'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:119: error: undefined reference to 'ReadJpegSectionsFromBuffer'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:121: error: undefined reference to 'create_EXIF'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:130: error: undefined reference to 'ReplaceThumbnailFromBuffer'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:140: error: undefined reference to 'WriteJpegToBuffer'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:141: error: undefined reference to 'DiscardData'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:168: error: undefined reference to 'IsGpsTag'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:170: error: undefined reference to 'GpsTagNameToValue'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:175: error: undefined reference to 'TagNameToValue'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:227: error: undefined reference to 'DiscardData'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:575: error: undefined reference to 'FindSection'

hardware/imx/mx6/libcamera2/JpegBuilder.cpp:609: error: undefined reference to 'FindSection'

collect2: error: ld returned 1 exit status

make: *** [out/target/product/sabresd_6dq/obj/SHARED_LIBRARIES/camera.imx6_intermediates/LINKED/camera.imx6.so] Error 1

 

Here is the JpegBuilder.cpp (excerpts; full JpegBuilder.cpp attached):

 

Line 118: ResetJpgfile();

Line 119: if (ReadJpegSectionsFromBuffer(jpeg, jpeg_size, read_mode)) {

Line 121: create_EXIF(table, exif_tag_count, gps_tag_count, has_datetime_tag);

Line 130: ret = ReplaceThumbnailFromBuffer(thumb, len);

Line 140: WriteJpegToBuffer(jpeg, jpeg_size);

Line 141: DiscardData();

Line 168: if (IsGpsTag(tag)) {

Line 170: table[position].Tag    = GpsTagNameToValue(tag);

Line 175: table[position].Tag    = TagNameToValue(tag);

Line 227: DiscardData();

Line 575: exif_section = FindSection(M_EXIF);

Line 609: exif_section = FindSection(M_EXIF);

 

Twelve errors total. The "JpegBuilder.cpp" is from the "kk4.4.2_1.0.0 GA" release. I do not know what is causing this. What do I do to fix this? Please help.

Thank-you,

 

Dave

ラベル(2)
0 件の賞賛
返信
0 返答(返信)