Kernel Source code 3.14.52 for imx6 sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel Source code 3.14.52 for imx6 sabresd

4,394件の閲覧回数
sijilpu
Contributor I

Hi

    I am trying to upgrade the kernel version 3.0 to 3.14 (for linux) in imx sabresd . I need  a kernel source code for this and   also want   to know the procedure for doing this. can you please provide the link for the kernel source code(3.14) that will support in imx6 sabresd board.

Thanks

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,970件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the attached document for the detailed information on how to install, build and deploy the 3.14.52 Linux BSP for i.MX6 series processors.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,970件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Here is the official repo:

linux-2.6-imx.git - Freescale i.MX Linux Tree

You should use this tag for 3.14:

linux-2.6-imx.git - Freescale i.MX Linux Tree

Note that 4.1.15 is now available too.

Regards,

Gary

0 件の賞賛
返信