Kernel Source code 3.14.52 for imx6 sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Source code 3.14.52 for imx6 sabresd

4,385 Views
sijilpu
Contributor I

Hi

    I am trying to upgrade the kernel version 3.0 to 3.14 (for linux) in imx sabresd . I need  a kernel source code for this and   also want   to know the procedure for doing this. can you please provide the link for the kernel source code(3.14) that will support in imx6 sabresd board.

Thanks

Labels (3)
0 Kudos
Reply
2 Replies

2,961 Views
art
NXP Employee
NXP Employee

Please refer to the attached document for the detailed information on how to install, build and deploy the 3.14.52 Linux BSP for i.MX6 series processors.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,961 Views
gary_bisson
Senior Contributor III

Hi,

Here is the official repo:

linux-2.6-imx.git - Freescale i.MX Linux Tree

You should use this tag for 3.14:

linux-2.6-imx.git - Freescale i.MX Linux Tree

Note that 4.1.15 is now available too.

Regards,

Gary

0 Kudos
Reply