Hi,
I tried to build Android KK4.4.3 image on my 32bit ubuntu14.04 host but error occured at lunch command.
It seemed x86_64 gcc(64b) used instead of i686 gcc(32b).
Can anybody help me to fix gcc selection as i686?
Thanks.
---
[Commands]
...
$ cd ~/myandroid
$ source build/envsetup.sh
$ lunch sabresd_6dq-user
$ make PRODUCT-sabresd_6dq-user 2>&1 | tee build_sabresd_6dq_android.log
[lunch error message]
/bin/bash: prebuilts/gcc/linux-x86/arm/arm-linux-androideabi-4.7/bin/arm-linux-androideabi-gcc: cannot execute binary file: Exec format error
[make error massages]
prebuilts/tools/gcc-sdk/../../gcc/linux-x86/host/x86_64-linux-glibc2.7-4.6/bin/x86_64-linux-ar only run on 64-bit linux
...
[Misc]
$ uname -sm
Linux i686
$ file prebuilts/gcc/linux-x86/arm/arm-linux-androideabi-4.7/bin/arm-linux-androideabi-gcc
prebuilts/gcc/linux-x86/arm/arm-linux-androideabi-4.7/bin/arm-linux-androideabi-gcc:
ELF 64-bit LSB executable, x86-64, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.8, stripped
解決済! 解決策の投稿を見る。
Hello,
In order to build android you need your host to be a 64 bit OS, that is why it's forcing you to use x86_64 gcc.
Also, I have never tried to build android with Ubuntu 14.04, it is recommended to use 12.04 as the latest.
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
In order to build android you need your host to be a 64 bit OS, that is why it's forcing you to use x86_64 gcc.
Also, I have never tried to build android with Ubuntu 14.04, it is recommended to use 12.04 as the latest.
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Sergio,
Thank you for your answer.
Finally I successfuly built KK4.4.3 images with 64bit ubuntu14.04.
P.S.
In my case, I added following package...
# http://source.android.com/source/initializing.html
$ sudo apt-get install bison g++-multilib git gperf libxml2-utils
# misc
$ sudo apt-get install gksu lib32z1 flex
and modified BoardConfig.mk to re-build boot.img for sdcard.
# $ make bootimage BUILD_TARGET_DEVICE=sd <== nothing changed!
$ vi device/fsl/sabresd_6dq/BoardConfig.mk
# <<del 13,18-23 lines>>
Have a nice day.
Thank you for giving us those details to set Android from Ubuntu 14.04!