Just add SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,278件の閲覧回数
farworld
Contributor I

Hello once again forum,

Just wanting to ask, is it possible I could just set the Sabre-lite, or a marsboard up to just boot from the micro SD?

If so, some actual instructions beyond 'Oh, look at the manual written for actual experts' would be nice.

ラベル(3)
0 件の賞賛
返信
1 解決策
3,173件の閲覧回数
EricNelson
Senior Contributor II
0 件の賞賛
返信
5 返答(返信)
3,173件の閲覧回数
farworld
Contributor I

So, you're saying that all I needed to do, was load the images onto the SD card and it would simply boot from them?

0 件の賞賛
返信
3,174件の閲覧回数
EricNelson
Senior Contributor II

Yes.

0 件の賞賛
返信
3,173件の閲覧回数
farworld
Contributor I

Thank you. You've pretty much just made my day with that.

0 件の賞賛
返信
3,173件の閲覧回数
EricNelson
Senior Contributor II

Glad to hear it.

Enjoy!

0 件の賞賛
返信
3,173件の閲覧回数
EricNelson
Senior Contributor II

Hi Luke,

What do you mean by "just boot from the microSD"?

The SABRE Lite essentially does that. What I mean is that all boot instructions are on the card in the boot script (6x_bootscript).

We have boot scripts that load Windows Embedded, Android, QNX, Yocto, Timesys, Ubuntu, Debian, et cetera and switch between them simply swapping cards.

You can also force the boot loader to load from SD, but this is a tricky operation, and recommended only for 'actual experts'...

0 件の賞賛
返信