Java with i.MX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Java with i.MX28

3,516 Views
alexandrglukhov
Contributor III

Hello, I have a problem, because I haven't enought experience. I have a single-board computer with i.MX28 with Linux, and I need to launch java programs (jre) on it. But I can't install java. Can somebody advise something about installing java with i.MX28?

Labels (2)
Tags (1)
0 Kudos
Reply
4 Replies

2,653 Views
Yuri
NXP Employee
NXP Employee

Please use the following from Community :

“All Boards Java”

https://community.freescale.com/docs/DOC-1478

Note, for i.MX28 we should use ARMv5 packages :

http://www.oracle.com/technetwork/java/embedded/downloads/javase/index.html


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,653 Views
alexandrglukhov
Contributor III

Thank you, but I meet another problems there:

If I need

Graphical ApplicationsARMv5 Linux - Headful (Early Access)EABI, glibc 2.5, Soft Float, Little Endian

then I download this one from Oracle

ARMv5 Linux - SoftFP ABI, Little Endian3101 MBhttp://download.oracle.com/otn/java/ejdk/8u6-b23/ejdk-8u6-fcs-b23-linux-arm-sflt-12_jun_2014.tar.gzejdk-8u6-fcs-b23-linux-arm-sflt-12_jun_2014.tar.gz

There are some "bin" directories with "java"

I put them on i.MX28, go to any of directory with java and write ./java -jar test.jar

So I get my Hello in console. But how to run program with visual forms, I get this error

Exception in thread "main" java.lang.UnsatisfiedLinkError: /ejdk1.8.0_06/linux_a

rm_sflt/jre/lib/arm/libawt_xawt.so: libXtst.so.6: cannot open shared object file

: No such file or directory

        at java.lang.ClassLoader$NativeLibrary.load(Native Method)

        at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1929)

        at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1814)

        at java.lang.Runtime.load0(Runtime.java:809)

        at java.lang.System.load(System.java:1083)

        at java.lang.ClassLoader$NativeLibrary.load(Native Method)

        at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1929)

        at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1835)

        at java.lang.Runtime.loadLibrary0(Runtime.java:870)

        at java.lang.System.loadLibrary(System.java:1119)

        at java.awt.Toolkit$3.run(Toolkit.java:1651)

        at java.awt.Toolkit$3.run(Toolkit.java:1649)

        at java.security.AccessController.doPrivileged(Native Method)

        at java.awt.Toolkit.loadLibraries(Toolkit.java:1648)

        at java.awt.Toolkit.<clinit>(Toolkit.java:1683)

        at java.awt.Component.<clinit>(Component.java:595)

Is it a problem with libXtst?

also Xfbdev on i.MX give this messages:

_XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6

_XSERVTransOpen: transport open failed for inet6/freescale:0

_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6

mxsfb_pan_display: var->xoffset 0, info->var.xoffset 0

mxsfb_check_var: xres 640, yres 480, bpp 16

get_matching_pentry: 480:640:16 vs 480:640:16

get_matching_pentry: 480:640:16 vs 480:640:16

mxsfb_pan_display: var->xoffset 0, info->var.xoffset 0

(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base

(EE) XKB: No components provided for device Virtual core keyboard

0 Kudos
Reply

2,652 Views
jamesbone
NXP TechSupport
NXP TechSupport

The error that you are having in the XFbdev it is because the FSL image for the i.MX28 does not have X11 support, you may need to add some X11 server first. I would also recommend that you contact the people from Oracle, since the BSP of the i.MX28 was made for Console Only. So that it is the case.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,652 Views
alexandrglukhov
Contributor III

Thank you, for answer

And how can I add X11 server? You mean select X11 in ltib -m config and select "build full modular X server"? If yes, I already select it, but still have the same error. How can I start it, if it's needed?

0 Kudos
Reply