JTAG Interface not as per IMX6SLHDG ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Interface not as per IMX6SLHDG ?

1,624 Views
pankajrana
Contributor III

Hi,

In the Hardware Dev. Guide for SoloLite - imx6slhdg.pdf document, there are recommendations provided for JTAG connections. But in the SoloLite Evaluation Kit schematics - MCIMX6SLEVK, the JTAG seems to be different.

term_rec.png

JTAG signals.jpg

  • For JTAG_TDO it is mentioned "Do not use pullup or pulldown" still a 10K option is provided (although it is DNP)
  • JTAG_TCK has On-Chip 47K pullup (can use 10K pullup optional), but in schematics a 10K pulldown is provided.

Please let me know the HDG vs EVK changes, what JTAG device can be used for MCIMX6SLEVK.

Should we follow the SL EVK schematics or refer the IMX6SLHDG ?

~Pankaj Rana

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,516 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

correct description gives Hardware Dev. Guide for SoloLite,

as for JTAG_TCK has On-Chip 47K pullup, R395 should be DNP.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply