JPEG encode/decode using Coda960 driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JPEG encode/decode using Coda960 driver?

3,095件の閲覧回数
jonathanolson
Contributor II

The CODA driver in the latest mainline kernel supports JPEG encoding/decoding for coda7 (imx5x) platforms, but does not support JPEG for coda960 (imx6) platforms.

The coda_regs.h header file does not even define the coda960 MJPEG registers starting at 0x3000.  Is there any support planned for the coda960 JPEG unit in the coda driver?  It appears that supporting JPEG on the imx6 should a straightforward port of code in the imx-vpu library.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,789件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Jonathan,

The gstreamer support JPEG with gstreamer1.0-plugins-base jpeg. the i.MX6Q does not have support for coda960 with imx.vpu library.

Regards

0 件の賞賛
返信

2,789件の閲覧回数
jonathanolson
Contributor II

The imx-vpu library https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-vpu-5.4.33.bin DOES support JPEG encode/decode on the i.MX6Q.  I've been successfully using this library for over a year with a 3.14 kernel.  There were gstreamer modules which also depended on this library,  however they cannot work on later 4.x kernels.

Unfortunately, the /dev/mxc_vpu device is deprecated in 4.x kernels and replaced with the new coda V4L2 driver.  Although the new coda driver supports H.264 encode/decode, it does not support JPEG on the i.MX6Q.  Since the imx-vpu library contains source code to manage the Coda960 jpeg hardware, I wondered if anyone has looked into porting this support into the coda driver.