Issues with serial on iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with serial on iMX6

1,211件の閲覧回数
bogdananton
Contributor I

Hello we use iMX6DP4AVT1AA  devices in a hardware setup running on windows7 32bit and libusbx-1.0.15-win 

We face some problems on the serial hardware, where we have a FTDI232RL + 3.3V level translation  to comunicate with the iMX chip  .

Sometimes the test system fails when waiting  for  iMX boot console response. 

Is there any hardware alternative to ftdi232rl chip for comunication with imx?

We tryied a alternative using the native COM1  via a max232 + optical isolation and level translation, but the results where worst 

Any sugestions?

Thank you

0 件の賞賛
返信
1 返信

1,164件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bogdan

from i.MX6 side there are no restrictions, one can use any rs232

converter or USB to serial UART interface.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信