Issues with Android Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with Android Boot

1,206 Views
anurag16doshi
Contributor III

I am using imx8mn board. I had a working Android boot img running. I made changes and redid the booting. I am working on Ubuntu 16.04 which is part of a dual booted PC. The allocated memory for the linux machine is 200+ GB. After remaking the kernel and boot images. My Ubuntu has run out of space. The main bulk of the memory is being used by .intermediate folder in <directory>/out/soong/.intermediate

 

I have used a procedure as mentioned in my previous post. https://community.nxp.com/t5/i-MX-Processors/Building-Android-BSP-with-RPMsg-enabled-for-iMX8-Nano/m...

 

I am uncertain of what the issue is. Could someone help understand the same?

 

TIA,

Anurag

0 Kudos
Reply
1 Reply

1,193 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Anurag16doshi,

The android BSP is not tested on ubuntu 16 you can try ubuntu 18, and it takes aprox 150GB, do not know exactly why it takes too much in your computer but you must deleted everything before compiled again.

 

Regards

 

 

0 Kudos
Reply