Issues with Android 5.1.1 on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with Android 5.1.1 on imx6

2,068 Views
davidwebster
Contributor I

I am currently trying to get Android 5.1.1 to boot up on a imx6 platform (solidrun i2ex SoM) by following the most recent guide from NXP.  I have a 800x480  7" LCD connected via a parallel RGB interface and can see the initial Android logo but never get to the home screen. I have attached the bootup log showing in logcat where it appears some errors occur with SurfaceFlinger towards the very end of the log.  Any assistance or suggestions would be greatly appreciated!

Original Attachment has been moved to: log_cubox_env_setup.log.zip

Labels (4)
0 Kudos
Reply
1 Reply

1,813 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

NXP BSPs support only NXP boards: Sabre SD, AI. For other boards

customization should be implemented by vendors of these boards.

It may be suggested to start porting this board with linux uboot logo,

for example below examples for various LCDs:

https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

Then port other drivers using attached Porting Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply