Issue with eth1 interface on imx6sx board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with eth1 interface on imx6sx board

1,311 Views
prasannakulkarni
Contributor IV

Hi all,

We are using IMX6SX Eval board and running Android 6.0.x marshmallow . we want use both eth0 & eth1 interfaces. but currently only eth0 interface getting UP on boot and eth1 manually we have to make it up. but dhcp is working only with eth0 not with eth1, even though both the interface are connected to diff dhcp servers. I have used the command "dhcptool eth1" after this it takes the ip from dhcp server. but the problem here is,  ping is not happening through eth1. what could be problem? and how to make both eth0 and eth1 both UP at the boot time with dhcp enabled? at the same time eth0 working in all cases.

1. After boot

# ifconfig

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope: Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 TX bytes:0

eth0      Link encap:Ethernet  HWaddr 00:04:9F:04:0D:1B
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 TX bytes:0

2. root@sabresd_6sx:/ # dhcptool eth1                                             
root@sabresd_6sx:/ # ifconfig                                                  
lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope: Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 TX bytes:0

eth0      Link encap:Ethernet  HWaddr 00:04:9F:04:0D:1A
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 TX bytes:0

eth1      Link encap:Ethernet  HWaddr 00:04:9F:04:0D:1B
          inet addr:192.168.1.102  Bcast:192.168.1.255  Mask:255.255.255.0
          inet6 addr: fe80::204:9fff:fe04:d1b/64 Scope: Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:9 errors:0 dropped:0 overruns:0 frame:0
          TX packets:15 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:1826 TX bytes:1706

root@sabresd_6sx:/ # ping 192.168.1.1                                          
PING 192.168.1.1 (192.168.1.1) 56(84) bytes of data. -----------stops.

Labels (1)
0 Kudos
Reply
0 Replies