Issue with adding OP-TEE support on i.MX 8MM venice

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with adding OP-TEE support on i.MX 8MM venice

4,036 Views
silentsky
Contributor I

Greetings,

I am having some troubles adding OP-TEE support to an i.MX8MM board. We are using the meta-freescale layer to provide optee recipes, along with a custom layer which provides a u-boot recipe.

 

I managed to get optee binaries installed, mainly using this presentation: https://timesys.com/webinars/Secure-by-Design-NXP-Webinar-Series-OP-TEE.pdf. The only thing left is getting /dev/tee* device to work, since for now it isn't even present. I tried to add a firmware node to the device tree in uboot-venice/arch/arm/dts/imx8mm.dtsi, and multiple other files in u-boot, but to no avail. I even checked that a .dtb file produced by yocto contains an optee node, but after booting the system it is not present.

I also tried inserting the firmware node to the system directly, in its own device tree, but then dmesg showed optee: api uid mismatch, which tells me that it should be added in u-boot.

Do you have any ideas what could be the cause of this problem?
Best regards,
Paweł

0 Kudos
Reply
1 Reply

4,009 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hi Pawel,

For more details about the installation I share the i.MX Porting Guide, chapter 5 is the configuration of OP-TEE

https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf

And the OP-TEE documentation, in the build and run section
https://optee.readthedocs.io/en/latest/building/index.html

 

Best Regards,

Diego.

0 Kudos
Reply