Issue about GPIO Value on MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue about GPIO Value on MX6DL

1,079件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     I want to check the key value in the recovery mode,and when I use the readl to read " GPIO3_BASE_ADDR + GPIO_PSR ", the val is 7fbf0000 and 5fbf0000,in other word ,I am  control the GPIO3-29,but our key is GPIO3-11, and why???

     please help me ,3Q~

ラベル(2)
0 件の賞賛
返信
1 返信

1,047件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

suggest to attach jtag and check register with oscillosope.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信