Is there any calculation tool of DRAM bus length for i.MX7ULP ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any calculation tool of DRAM bus length for i.MX7ULP ?

785件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

 

I'll building a custom board with i.MX7ULP.

I understand that the wiring of each DDR signal line (the wiring from the CPU BGA pad to the DDR BGA pad) must be of equal length.

 

Is there any information about the wiring length inside the CPU (the wiring length from the DDR controller inside the CPU to the BGA PAD) ?

Or is there any calculation tool of DRAM bus length for i.MX7ULP ?

I found following check sheet but it's for i.MX6.

https://community.nxp.com/docs/DOC-93819

 

Ko-hey

ラベル(1)
0 件の賞賛
返信
1 返信

734件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   It is recommended to use section 3.4.1 (DDR routing rules) of the

Hardware Development Guide for the i.MX 7ULP.

https://www.nxp.com/webapp/Download?colCode=IMX7ULPHDG 

It is quite enough for practical purposes.

Regards,

Yuri.

0 件の賞賛
返信