Is there a documentation of Android M bsp development ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a documentation of Android M bsp development ?

2,370件の閲覧回数
ganyeking
Contributor II

hi community:

Recently,i should fit android M driver for my custon-board ,it's relay on imx6q .Then,Does NXP provide like Androind M bsp development of technical documentation?

Best Regards

ganye

ラベル(4)
0 件の賞賛
返信
4 返答(返信)

2,094件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ganye

specific i.MX documentation is included in android doc bundle

http://www.nxp.com/webapp/Download?colCode=IMX6_M6.0.1_2.1.0_ANDROID_DOCS&Parent_nodeId=133769948107... 

there is no general android porting guide, one can refer to common android developers resources.

As android is based on linux, it may be useful to check linux porting guide included in

linux doc bundle

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,094件の閲覧回数
ganyeking
Contributor II

Hi igor

Thank you for your prompt reply.Now ,I would like to learn more about Android M driver development, what book do you have any recommend books for me?

Thank you in advance.

Best Regards

ganye

0 件の賞賛
返信

2,094件の閲覧回数
ganyeking
Contributor II

Hi igor

Thank you very much.

Best Regards

ganye

0 件の賞賛
返信