Is there RT Linux support for i.MX28 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there RT Linux support for i.MX28 ?

2,558件の閲覧回数
richardtseng
Contributor I

Dear all,

Have anyone tried running RT Linux on i.MX28 ?

It seems RT Linux patch is only available for 2.6.33, but i.MX28 Linux is based on 2.6.35:

https://www.kernel.org/pub/linux/kernel/projects/rt/

Is there a Linux 2.6.31 BSP for i.MX28 ?

Thanks,

Richard

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,118件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You can use kernel 3.10 (or also 3.12 when the RT patches become availble) on mx28.

Regards,

Fabio Estevam

2,118件の閲覧回数
richardtseng
Contributor I

Hi Fabio,

Where can I download Linux 3.10 for i.MX28 ?

Richard

0 件の賞賛
返信

2,118件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Richard,

You can get it from kernel.org

git://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-stable.git

And then use a 3.10 branch.

Regards,

Fabio Estevam

0 件の賞賛
返信