Is the IO voltage of the QSPI specified by the NVCC_NAND supply voltage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the IO voltage of the QSPI specified by the NVCC_NAND supply voltage?

ソリューションへジャンプ
705件の閲覧回数
t-iishii
Contributor II

Hi,

In IMX6ULL,

Is the IO voltage of the QSPI specified by the NVCC_NAND supply voltage?

Best regards,

Ishii.

タグ(2)
0 件の賞賛
返信
1 解決策
639件の閲覧回数
art
NXP Employee
NXP Employee

Yes, on the i.MX6ULL processor, the NAND and QSPI interfaces share the same I/O pads that are supplied by the NVCC_NAND power rail.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
640件の閲覧回数
art
NXP Employee
NXP Employee

Yes, on the i.MX6ULL processor, the NAND and QSPI interfaces share the same I/O pads that are supplied by the NVCC_NAND power rail.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信