Is the IO voltage of the QSPI specified by the NVCC_NAND supply voltage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the IO voltage of the QSPI specified by the NVCC_NAND supply voltage?

Jump to solution
704 Views
t-iishii
Contributor II

Hi,

In IMX6ULL,

Is the IO voltage of the QSPI specified by the NVCC_NAND supply voltage?

Best regards,

Ishii.

Tags (2)
0 Kudos
Reply
1 Solution
638 Views
art
NXP Employee
NXP Employee

Yes, on the i.MX6ULL processor, the NAND and QSPI interfaces share the same I/O pads that are supplied by the NVCC_NAND power rail.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
639 Views
art
NXP Employee
NXP Employee

Yes, on the i.MX6ULL processor, the NAND and QSPI interfaces share the same I/O pads that are supplied by the NVCC_NAND power rail.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply