Is it possible to interface two displays with MIPI interface and Two Cameras with MIPI CSI at the same time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to interface two displays with MIPI interface and Two Cameras with MIPI CSI at the same time?

2,903件の閲覧回数
shree97
Contributor II

Hello Community,

I want to interface two displays using MIPI interface with i.MX6 Solo and these displays should work at a time with different output.Also the same with the cameras.

I read the i.MX6 solo reference manual but I didn't find any clue(or it may be I didn't understand) . Is this possible with i.MX6 solo?

Best Regards,

Shree

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,400件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  As for multiple cameras support, please use the following :

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

 

For 4xMIPI case, the four cameras should be combined (using external circuit) on the single

MIPI CSI2 interface, and each camera data should be transferred on a MIPI virtual channel.

 

  For MIPI DSI - the source of MIPI DSI is one IPU DI, so there is only one group of display timing

input to MIPI DSI. No several displays support.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信