Is ODT(on-die termination) not necessary for T topology?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is ODT(on-die termination) not necessary for T topology?

1,533件の閲覧回数
王剑翰
Contributor III

In IMX6SLHDG.pdf, Page 30:

2.5.2 DDR3 (32 bits) T topology considerations

Be sure to take into account the following when designing a T-topology system.

• Follow the routing rules described in  Table 2-3 .

• Termination resistors not required.

• Short routing lengths and on -chip drive strength control.

• Your design is limited to 4 DDR chips.

• DDR3, 2 GBytes using latest memories (4 GBytes coming).

As above claimed,  termination resistors is not necessary for T topology. So ODT is NOT required for T topology? I can not understand it. Please kindly explain it or correct me if my understanding is wrong. Thank you!

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,270件の閲覧回数
王剑翰
Contributor III

I have got the answer.

0 件の賞賛
返信

1,270件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

OK, so we are closing your question.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信