Internet on IMX6 quad core with pre-loaded android image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internet on IMX6 quad core with pre-loaded android image

869 Views
danielromero
Contributor I

I cannot get the internet to work on an IMX6 quad core demo board. Is there wifi on the board? I am also plugged into the ethernet port. Is this supported on the pre-loaded android image? Thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

732 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Daniel Romero,

It does support the ethernet. About wifi you need to confirm if there is wifi module in the board.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply