Interface an external RAM with i.MX RT 1062

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interface an external RAM with i.MX RT 1062

2,286件の閲覧回数
biccius
Contributor I

Hello everybody,

I was asked to make a project which requires the fastest access possible to a RAM (write and read).

I am still in a study phase and at the moment it seems to me that the SEMC interface on a i.mx rt 1062 allows to do this.


Has anyone already had experience of this and if so, what type or model of RAM have you used and with what performance?


Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

2,092件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Use the following app note:

“i.MX RT Series Performance Optimization”

 

https://www.nxp.com/docs/en/application-note/AN12437.pdf 

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信