Inter processor communication (Between iMX8MQ and i.MX8MQ) design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inter processor communication (Between iMX8MQ and i.MX8MQ) design

1,514件の閲覧回数
harshitshah
Contributor III

Hi NXP Team,

We are planning to establish an inter-process communication between two i.MXMQ series processors.

  • Approach-1:
    • The first approach is to establish connectivity via MAC(RGMII) interface. 
  • Approach-2:

Queries:

  1. In the i.MX6Q references the results mentioned below. Will we get similar results in i.MX8Q? pastedImage_4.png
  2. What throughput we can expect in approach 1? (Using RGMII connections?)
  3. Which design is better for inter-process communication between two processors(The communication would be of non-video data)? 

Regards.

ラベル(2)
0 件の賞賛
返信
1 返信

1,446件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harshit

1. yes

2. i.MX8MQ has not rgmii issues/errata, so rgmii performance can be obtained

3. seems for short distance pcie is better (less wires), for longer distances probably

rgmii better as it imposes less requirements on board/cable/connectors quality

to avoid signal loss.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信