Inquiry MMPF3000 Coin Cell charger control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Inquiry MMPF3000 Coin Cell charger control

1,768 次查看
andychien
Contributor III

Dear Sir,

Our customer used i.MX6UL+ PF3000 and add coin cell to design product.

We knew if system off (PMIC Vin off), coin cell provide power to VSNVS of i.MX6UL then work RTC function only.

If PMIC Vin provide power and system work, we will setting COINCTL register (COINCHEN bit) to enable charger coin cell.

We are not sure how to control disable or know coin cell is full to stop charger.

Could you help provide control method, software or circuit to reference?

Thanks a lot, 

标签 (2)
0 项奖励
回复
2 回复数

1,546 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andy

coin cell charger voltage is programmable as described in

sect.6.3.11.4 Coin cell charger control datasheet. It works as

current-limited voltage source, resulting in the CC/CV taper characteristic

typically used for rechargeable Lithium-Ion batteries. So no need

 to stop charger current as it stops automatically as cell voltage reaches

programmable level.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,546 次查看
andychien
Contributor III

Thanks Sir,

I will tell customer to confirm coin cell Vendor.

If any question, we will tell you.

Thanks for fast help

0 项奖励
回复