Init scripts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Init scripts

1,828 Views
vishakh
Contributor III

Hi,

I am using i.MX6q based platform running Linux 3.0.35 and Barebox boot loader.

Here Linux is not executing the "/etc/rc.d/ " scripts automatically. I am able to run these scripts manually.

But, when I boot Linux using u-boot, Linux executes these scripts automatically.

Can someone help me to solve this?

Thanks and Regards,

Vishakh

Tags (3)
0 Kudos
Reply
2 Replies

1,686 Views
jimmychan
NXP TechSupport
NXP TechSupport

have you try /etc/init.d/ ?

0 Kudos
Reply

1,686 Views
vishakh
Contributor III

Thank you for the reply.

Rootfs doesn't has /etc/init.d/, but instead has /etc/rc.d/init.d/.

But these scripts too not executing.

0 Kudos
Reply