Increasing PMIC current sourcing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Increasing PMIC current sourcing

1,196件の閲覧回数
surendrajadhav
Contributor IV

Hi,

Can we short SW1A output (i.e.DCDC_3V3) and SW2 output (i.e.VPERI_3V3) together, in order to increase the total current capacity of the 3.3V power rail.

Will it impact the power Up and Down sequence of the CPU. This is shown below.

PMIC.PNG

Regards, Surendra

ラベル(2)
0 件の賞賛
返信
1 返信

1,132件の閲覧回数
art
NXP Employee
NXP Employee

No, it is not possible to do it the way you describe due to the asynchronous nature of these switching regulators operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信