Inconsistency in I2C Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Inconsistency in I2C Interface

跳至解决方案
1,652 次查看
sachinmohankura
Contributor I

Hi,

We notice inconsistency in data received from touch controller.

  • We get valid data for few cycle
  • We get data read error for few touch input
  • We get NAK for data read from touch after address cycle.
  • We get ACK for the data but data read is FF all the time( here the I2C clock is held low for one or more cycle in between 8 bit read)

 

I have summarized all data in Touch panel I2C Issue.PPT and LA waveform capture(PNG Image).

Regards,

Sachin

0 项奖励
回复
1 解答
1,580 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sachin

issue may be caused by signals noise or operating systems delays, so one can try to

decrease operating i2c frequency, add delays and descrease pull resistors values.

May be recommended to try with baremetal sdk (or freertos)

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,581 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sachin

issue may be caused by signals noise or operating systems delays, so one can try to

decrease operating i2c frequency, add delays and descrease pull resistors values.

May be recommended to try with baremetal sdk (or freertos)

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复